Other Parts Discussed in Thread: ONET8501V
There are 3 fault conditions in ONET8501V Datasheet as below, however, if the bias current is very small e.g. less than the minimum bias current, it also can trigger the fault. Can Great TI support provide more detailed ONET8501V fault condition? thanks.
1. Voltage at MONB exceeds the voltage at RZTC (1.15V),
2. Photodiode current exceeds 150% of its set value,
3. Bias control DAC drops in value by more than 50% in one step.