I am configuring our USB IP as USB 2.0 only and using it on zynq 702 board for testing with TUSB1310A phy . Every time i try to connect a USB2.0 device i get message of "USB 1.1 new low speed device connected" . Please help me out here.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Shweta,
I will check the info and I will come back to you soon.
Regards,
Gerardo
Hi Shweta,
Everything looks fine,
Can you send the schematic at TUSB1310 section in order to take a look on it?
Regards,
Gearado
Hello Gerardo ,
The problem is solved now Actually the issue was in addon we were using to connect the device.
Thanks and Regards,
Shweta
Hello,
Currently the addon board which we are using have DP,DM connections cross connected. Thus , DP of host (from TI Phy) is connected to DM of Device .
Now the analyzer is able to detect SOF packet but i have doubt whether that SOF will reach device end in same format ?
Hello Shweta,
Glad to see that the issue is solved now.
Please open a new post for the additional questions.
Regards,
Gerardo