Other Parts Discussed in Thread: SN65HVS880, CD54HC166, CD74HC166, SN65HVS885
Hello Team,
I was taking a look at the SN65HVS88x devices for a system I'm working on that needs an 8-input digital serializer that is approximately compatible with 5V CMOS logic and can tolerate inputs up to 24V.
I believe that the SN65HVS880/5 is capable of handling part of this requirement (8-input and 24V tolerant), but I don't think it will meet the logic detection requirement.
My understanding is that the 'Field Input (low/high)-State Input Voltage' spec determines when a '0' or '1' will be triggered by an input, and this is off for both.
Are there any serializers that would meet all of my requirements? Is there perhaps an alternate route that I should consider for handling both?
Best Regards,
Ben