Other Parts Discussed in Thread: DP83849IF
I am using the DP83849IF Dual-Phy and want to use the Strap Options for automatic configuration during start-up. I am using actually an microblaze prozessor to set the register using the MDIO interface.
First I readout the actual register status and then I set the register and read out the register status again.
I can see that using the strap options nearly everything is alreight but in register 4 bit 7 (100BASE TX-Support) is 0 instead of 1. I have tested several strap options to set these bit to 1 but I have no idea which strap option I have to use.
I can´t find in datasheet an table with the corresponding strap options to a register.
If anyone now how to do this, please help.