Other Parts Discussed in Thread: DP83816
Hello,
with our current design, ethernetcard with two DP83816, we encountered troubles, when using it with EtherCAT.
We receive many symbol errors, ... . Our design is based on the reference schematic from the NSC-Demoboard, Doc.Nr. 870011508-300.
After checking the latest datasheet, i saw, that the receive path, shown on page 101, is different compared to the NSC-Demoboard.
( centertap of receive must now be connected to VDD, the centerpin of the two resistors must also be connected to VDD, an the
value of the resistoers changed from 54.9Ohm to 49.9 Ohm )
Can someone tell me, which circuit is now the correct one ?
best regards,
Peter