Other Parts Discussed in Thread: P82B96, TCA9517
The VOL of Sx/Sy of P82B96 is around 0.8 V. I would like to reduce it to 0.4 V maximum. Any kind of solution? Cascade another chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rajan,
The datasheet of TCA9517 says:
The B-side drivers operate from 2.7 V to 5.5 V. The output low level for this internal buffer is approximately 0.5 V, but the input voltage must be 70 mV or more below the output low level when the output internally is driven low.
Is it will be a problem if we connect B-side to Sx/Sy of P82B96?
F.Z.