This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV031 Variations in an input signal

Hello,

There is undershoot in input signal (DINx) of DS90LV031.

Is there any acceptable level of undershoot?

Best regards,
Seishin

  • Seishin,

    Technically this waveform violates the absolute maximum condition for a short period during the transition from high to low.  However, very short duration low voltage events like the one shown on the oscilloscope waveform above do not present a reliability concern for the input structure.

    Good system design practices like series termination resistors can minimize and even eliminate most undershoot or overshoot conditions. 

    I would highly recommend series termination for undershoot events which last for > 20 ns and/or have an amplitude of -0.8V or VDD+0.8V

    Regards,

    Lee