Other Parts Discussed in Thread: TPS25810, TPS25810EVM-745
Hi all
Would you minf if we ask TPS25810?
Do CC1 and CC2 have reverse protection?
We can't find it on the datasheet.
Kind regards,
Hirotaka Matsumoto
TPS25810
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS25810, TPS25810EVM-745
Hi all
Would you minf if we ask TPS25810?
Do CC1 and CC2 have reverse protection?
We can't find it on the datasheet.
Kind regards,
Hirotaka Matsumoto
TPS25810
The datasheet is currently getting updated. When it is complete it will have an updated section for ESD Ratings as shown here.
ESD Ratings
|
|
VALUE |
UNIT |
|||
|
V(ESD)(1) |
Electrostatic discharge |
Human-body model (HBM), per ANSI/ESDA/JEDEC JS-001(2) |
±2,000 |
V |
|
|
Charged-device model (CDM), per JEDEC specification JESD22-C101(3) |
±500 |
||||
|
IEC(4) |
IEC61000-4-2 contact discharge, CC1 and CC2 |
±8,000 |
|||
|
IEC61000-4-2 air discharge, CC1 and CC2 |
±15,000 |
||||
(1) Electrostatic discharge (ESD) to measure device sensitivity/immunity to damage caused by assembly line electrostatic discharges into the device.
(2) JEDEC document JEP155 states that 500-V HBM allows safe manufacturing with a standard ESD control process.
(3) JEDEC document JEP157 states that 250-V HBM allows safe manufacturing with a standard ESD control process.
(4) Surges per IEC61000-402, 1999 applied between CC1/CC2 and output ground of the TPS25810EVM-745
Lee san
Thank you for your reply.
And, we are sorry that our explanation is not enough.
"Do CC1 and CC2 have reverse protection?"
->This means whether CC1 and CC2 have reverse protection for current or not.
So, as abnormal situation, if IN2 is not supplied, CC1 and CC2 are supplied the voltage, is it not problem?
Kind regards,
Hirotaka Matsumoto
As long as IN2 is under UVLO the internal fet will remain in the off state and no current will flow in reverse direction into IN2.