Other Parts Discussed in Thread: DS15EA101, DS15BA101, DS25BR110, DS25BR120
Dear Sir,
I have a prototyp board with an FPGA two DS15BA101 and two DS15EA101.
My target is to send data out of the FPGA (LVDS 2,5V) to the DS15BA101. From there AC coupled (1uF) over a Ethernet cable back to the AC coupled (1uF) DS15EA101.
When I send a endless data stream (200MBit/s) with the bit-sequence "0101010101", I also get "0101010101". That's fine.
But If I send "0110010101" I receive "0111010101". And the wrong "1" is also stable. I don't know why that happens.
Hope you have some ideas.
Are there some rules to follow when sending a data stream?
Thanks,
Martin