Other Parts Discussed in Thread: TPS65982, TPS6598X-CONFIG
Hi all
Would you mind if we ask the function of TPS65982 and TPS65986?
Our customer is looking for UFP Type-C with PD device with following spec.
<Spec>
-It is possible to operate the device without CPU.
-After 20V is supplied, the system power is ON with DCDC converter via FETs of HV_GATE1 and HV_GATE2.
So, is it possible to adjust the threshold of HV_GATEX operation using Configuration tool?
-If it occurs OCP, the voltage switches off.
-They don't use USB signal.(Only PD device)
So, as USB-PD power switcher with CC contorl, is TPS65982 fittable?
kind regards,
Hirotaka Matsumoto