Other Parts Discussed in Thread: TMDS171
Hi team,
I have automotive customer that's making one Hub project, that would have one HDMI input port, and there is a device /MAX9293 transmitting the HDMI signal to GMSL output interface.
The HDMI cable from other peripherals connecting to this Hub/HDMI, is unknown yet. And the Hub PCB size is around 75mm *75mm.
So we are thinking if one HDMI retimer like TMDS171 would need to be added.
Could you help share more the application conditions HDMI retimer is required, like cable length, data rate, etc ?
Does HDMI qualification test also need adding retimer to pass?
Thanks.