Other Parts Discussed in Thread: TUSB7340
We are having issues with a TUSB7340 blues screening when a pcie to usb ethernet is attached. This is part of a socking station. It appears as if the hub is waiting on the ethernet device to disconnect which it never does because it was removed. Issues only seem to happen on windows 7, windows 10 seemed to appear ok. We also have an issue when removing the device in sleep and waking the computer. Devices are never removed. Bios ACPI section is in place for the dock disconnect and wake portion. - Jim