Other Parts Discussed in Thread: TUSB9261, TPS2561, TPS2560
Hello,
I'm going to be implementing a single USB connection to 4 SATA devices (using the a single USB to 4 hub, and then 4x TUSB9261), please note that this will be for USB2.0, not 3.0 (which I believe I can still use the TUSB9261, as this still has compatibility to USB2.0 Highspeed.
When reading the implementation pdf, the TUSB9261 is connected to a TPS2561, and that this is enabled via GPIO10. Correct me if i'm wrong but isn't GPIO10 initially undefined with default firmware. Does this mean that when implementing the TUSB9261, I'll need to update the firmware? If so how do I do this?
Additionally, when using multiple SATA devices, will each SATA connection require 1 TPS2561, or can this be connected to 2 SATA connections?
Regards,
Thomas