Other Parts Discussed in Thread: TFP410
Hi there,
I am using the TFP410 on a Prototyp Board wich i intend to use for testing the RGB TTL Display-Output on our Industrial-PCs.
Now i figured it only works when i run it for about 5-10min and it gets "warm". At normal room temperature (22°C) i get nothing on the DVI outputs.
I used Cooling Spray to reproduce the conditions, but when its farly cooled down it works again! So it only don't work in a specific temperature range around 20°C.
I use the device without I2C, and i think i have all the settings right.
The video input is 800x480 with 29.55MHz Pixel Clock.
i can provide the schemtics, if needed.
Any Idea?
Hans