Other Parts Discussed in Thread: TUSB1310A
Hello ,
Currently in our design we are using zynq702 board with TUSB1310A phy for USB 2.0 host testing. As our TUSB1310A board is having type B Connector , we are using add-on board to connect device to the host. In the addon board the DP/DM are swapped . Thus host's DP is connected to device's DM and vice verse.
The analyzer in between host and device decode the SOF and SETUP packets , but i have doubt regarding data received at device end. Moreover would TUSB1310A will decode the sync/EOP pattern from device correctly ?
Regards,
Shweta