Other Parts Discussed in Thread: TUSB2036
I'm getting the "Device Not Recognized" message while trying to connect my PC (Windows 7 Professional). I've checked other threads in the TI forums but I don't see anyone trying to use the TUSB2036 in a self-powered design. I'm attaching a PDF of my schematic. I'm only using two ports. The first port goes directly to an Atmel micro-controller USB port. The second port goes to an FTDI USB to UART chip. Both are always connected. I'm not using external memory and I'm using a 48 MHz clock oscillator connected directly to the TUSB2036 (extremely close...very short trace from clock output to the TUSB2036). I'v tried connecting after power-up, connecting before power-up, and even forcing a reset after power-up and connection. I always get the same error message. Any help would be most appreciated.