Other Parts Discussed in Thread: HD3SS460, TIDA-00714, TPS65982
I think I've read through all the relevant posts on this subject. My requirement is to create a device that is:
- fitted with a USB 3.1 Type C receptacle
- Has a microcontroller that runs USB 2.0
- Has a FPGA that outputs DisplayPort 1.2 (2 lanes will work but I think 4 is possible due to the USB only being 2.0)
- Which can support:the following functionality:
- Sink power from the device attached (5V at < 1 Amp is more than enough)
- Provide power to the device attached (but only a USB drive is envisioned at present)
- Communicate over a USB 2.0 connection with a remote device
- Source a DisplayPort 1.2 signal to an attached device (the max resolution we envision right now is 1920 × 1080 × 24 bpp @ 60 Hz)
Given that I don't need Thunderbolt support, I think the TPS65986 will be the right choice but do I need to include a HD3SS460 SS Mux IC too as shown in Fig 78 of the TPS65986 datasheet or will the internal Mux work OK for my requirements?
Any starting point schematic to base my design from would be a huge help - I think the TIDA-00630 Dock solution is the right one IF I need the external SS MUX but, if not, maybe the TIDA-00714 solution will work.