Other Parts Discussed in Thread: DS90UB947-Q1, DS90UB948-Q1
Hello,
If the sensor & ISP is Sony IMX290 (1080P) + CXD5700. Which SerDes IC do you suggest to match CXD5700 ? Thank you.
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90UB947-Q1, DS90UB948-Q1
Hello,
If the sensor & ISP is Sony IMX290 (1080P) + CXD5700. Which SerDes IC do you suggest to match CXD5700 ? Thank you.
BR
Patrick
Hi Patrick,
If you are using a 1080P camera using YCrCb on the CXD5700 16-bit output (according to the block diagram I have found below), my estimation is that you will need a device that is at least 16 bits wide at approximately PCLK = 150 MHz:
I can only think of an FPD-LINK III solution for this, such as the DS90UB947-Q1/DS90UB948-Q1 pair.
Regards,
Michael