This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EFT and Surge protection of TRS3243E 232 transiever



I see where the device is protected against IEC61000-4-2 level 4 ESD. Is there a level of IEC61000-4-4 EFT or IEC61000- 4-5 Surge protection?

thanks