Hi,
We would like to connect the IMX123 Sony sensor to a DM8147 DSP.
Our presen solution use different Aptina sensors in HiSPI mode, and we use the interface chip SN65LVDS324.
- Can we connect the IMX123 sensor to LVDS324 in the 4ch LVDS mode?
- Are there any idea how can we connect the IMX123 to DM8147?
(We cant find detailed information about the allowed packet structure of the LVDS324, but I think it should conform with the HiSPi specification. And we understand, that the IMX123 can provide MIPI/CSI-2 output, but our present receiver module in mass production use the LVDS324 receiver, which translates the HiSPI to parallel data for the DM8147, and the CSI-2 receiver of the DM8147 is not documented,)
We are appreciate any answer.
Best regards,
Gabor Fancsali