This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK1201 external PRBS loopback



Hello there!

I have a question about TLK1201 Ethernet transciever. It has an internal PRBS generator so I'd like to use it to test the device and a link. In the datasheet I've found information that I can connect TX output to a bit error rate tester or to the reciever of another TLK1201.

So the question: Is it possible to connect TX with RX of the same device and to orginize external PRBS loopback?

Best regards, Alexey.