Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCI2050B GHK/ZHK package NC pins?

Other Parts Discussed in Thread: PCI2050B

The most recent datasheet labels many pins "NC" for the GHK/ZHK package. Unfortunately, there isn't even a footnote defining NC as "No Connect", and if there were, "No Connect" is a vague term that can be interpreted in 2 distinct ways with opposite implications for an EMI/EMC/SI expert reviewing my design. He wants me to tie off every single ball on the package that is not used for signal or power.

1) NC could mean that the balls are not connected anywhere and it is safe to tie them to ground.

2) NC could mean "Do Not Connect", there may be test signals on some of these balls.

My question is:

Is it safe to tie all the NC balls to ground for the PCI2050B GHK/ZHK package?

Best regards,

A careful engineer burnt too many times by Murphy's law.