Other Parts Discussed in Thread: HD3SS6126EVM, HD3SS6126
Hi all,
I am working on usb 3.0 2:1 Mux , part no is HD3SS6126. It has on evaluation board which part no is HD3SS6126EVM.
There is pin mismatching in part data sheet and evaluation board reference design.
In Datasheet see the page no 3 and In reference design of evaluation board document see the page no 5.
In reference design Pin 3 SEL1 , Pin 9 SEL0 , Pin 6 HS_OE0, Pin 41 HS_OE1
In Datasheet Pin 3 NC Pin 9 SEL , Pin 6 HS_OE, Pin 41 NC
which one is correct datasheet or reference design ?
and what is the logic of two SEL0,SEL1 pin and same as two HS_OE0 ,HS_OE1 ?
Data sheet link :
Reference design Note :
http://www.ti.com/lit/ug/slau541/slau541.pdf
Thanks,