Other Parts Discussed in Thread: TPS65982, TUSB8041
Hello,
Instead of routing the separate USB 2.0 D+/D- top and bottom pairs to TPS65982, is there any issue with shorting top/bottom together at the connector, and routing the single pair to the IC?
If not, does it matter whether this merged pair is routed to C_USB_TP/N or C_USB_BP/N?
This is with a UFP, DP-sink application in mind. Figure 44 of the TPS65982 datasheet shows both the top and bottom USB 2.0 paths routed to the same crosspoint mux in the Digital Core, so I assume it's irrelevant whether this single pair is routed to C_USB_TP/N or C_USB_BP/N. But I'm not clear whether there is any functionality that is lost by doing this. It'd be preferred from a board space savings and ESD perspective.
Thanks,
Jonathan