Other Parts Discussed in Thread: DS250DF810
Hi ,
I would like to ask a question regarding to the ds250df810 retimer.
The datasheet states that Each channel of the DS250DF810 independently locks to serial data rates in a continuous range from 20.6 Gbps to 25.8 Gbps or to any supported sub-rate (÷2 and ÷4), including key data rates such as 10.3125 Gbps and 12.5 Gbps, which allows the DS250DF810 to support individual lane Forward Error Correction (FEC) pass-through.
My plan is to use the ds250df810 retimer between an FPGA and an SFP+ connector. The transceivers of the FPGA, support 16.3Gb/s.
My question is: does the retimer supports the 16.3 Gb/s bandwidth?
Thank you!