Other Parts Discussed in Thread: HD3SS460, TPS65982, TPS6598X-CONFIG
Hi team,
Customer is designing POS and plan to add type C PD into their design to support 5V 3A, 12V 3A and 20V 5A, USB HS and SS.
We are promoting TPS65982 + HD3SS460 to customer. Some questions from customer need your help to answer.
1. With config. ID 0 (S1=0000), same setting on both end, what happen when adapter is plugin into both EVM?
2. Need confirmation TPS65982 will not effect USB HS and SS enumeration?
3. Is there a config. which allow sink and source 20V @5A, 12V @3A, 5A @3A? 100W is the priority.
Customer like to have 20V @5A to supply from their system to device, and device to system whenever adapter is plugin, and the type-C connector support standard type-C peripheral as well.
Both system and device will design in TPS65982+HD3SS460 on each end. Thank you for your advice.
regards, Ken