Hello,
We have the following setup: x8 wide PCIe Gen 3.0 connection as follows
PLX9733 -> connector & PCB -> DS80PCI810 -> connector & PCB & external 3 ft cable -> connector & PCB -> DS80PCI810 -> connector & PCB -> PLX9797.
I have successfully set this path up for x8 Gen 1, x8 Gen 2. When I try to get Gen 3 working, I can only succeed if I limit the width to x1 only (by powering down the other 7 lanes).
When I try to go to x2 wide (or wider), the PLX Receiver Error and Recovery State counter registers quickly reach their maximum values.
I have tried a wide variety of settings for eq, VOD, and VOD_DB and cannot eliminate these errors.
Are there recommended values for running two DS80PCI810's in series? Or, are there any reserved register settings that I can use to disable the EQ and just pass through the input for debugging in order to eliminate one of the '810s?
Thanks