This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI402SQE LPBK pin function

Hola,

May I know what's the function of the LPBK pin?

This device has 4 lane but its adjustable pin of the EQ and DEMB only has two setting.

ex:EQA1, EQA0, DEMA1, DEMA0

May I know that how can I adjust these 4 lane by using EQ and DEMB?

  • The loopback pin (LPBK) can be used to create a loopback path from INA - OUTB or INB - OUTA based on the input level shown in the table above.

    There are EQA[1:0] and EQB[1:0] pins which control INA_n and INB_n inputs respectively.  Using the pins to control the equalization level gives 16 possible settings for each group of pins.

    There are DEMA[1:0] and DEMB[1:0] pins which control OUTA_n and OUTB_n outputs respectively.  Using the pins to control the de-emphasis level gives 16 possible settings for each group of pins.

    Additional control is possible using the ENSMB pin.  When using pin controls ENSMB = GND, if ENSMB = HIGH then additional control can be achieved on a per channel basis with SMBus registers.

    Regards,

    Lee

  • Hola Lee,

    Great and helpful. Thank you very so much.