This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620 : Optical fiber connector length

Guru 19685 points

Other Parts Discussed in Thread: DP83620

Please let me know about max length of optical fiber connector on DP83620.

・Customer information

 ・Optical fiber connector name : AFBR-5972Z (Avago)

 ・DP83620 ~ Connector pattern length is 150mm

Best regards,

Satoshi

  • Satoshi,

    Could you clarify your question?  Are you asking about the physical size of the fiber optic transceiver? 

    The AFBR-5972Z supports LVPECL levels and has a signal detect output.  It should be interoperable with the DP83620.

    Patrick

  • Patrick-san

    Sorry for unclear question.

    For customer reason, circuit board of DP83620 and AFBR-5972Z are difference.
    Distance of two boards is 150mm.
    Customer is worrying that 150mm is no problem or NG.

    Best regards,
    Satoshi
  • Satoshi,

    The fiber interface has not been validated over 150mm. It is theoretically possible, but would need to be evaluated by the customer in their system, especially given that we cannot guarantee the functionality of the AFBR-5972Z over that distance.

    Note that there is more flexibility on the trace lengths for the MAC interface. Perhaps they could increase the distance between the MAC and the PHY to decrease the distance between the PHY and the fiber optic transceiver.

    Patrick