This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is looking for a repeater and/or switch devices for FPD-Link III signal in between DS90UB913A and DS90UB914A.
Can you help me to find out good suggestion from broader line-up?
* Test purpose (not for production)
* one camera (DS90UB913A)
* four DS90UB914As
* No back channel communication required
* Differential STP
* No Power Over Cable
* See drawing below
As long as I checked some devices, I have found following devices.
DS25CP104A / DS25CP114
3.125 Gbps 4x4 LVDS Crosspoint Switch with Transmit Pre-Emphasis and Receive Equalization
SN65LVCP402
Gigabit 2x2 CROSSPOINT SWITCH
DS25BR204
3.125 Gbps 1:4 LVDS Repeater with Transmit Pre-Emphasis and Receive Equalization
Do you have any other suggestion that can be recommended?
Thanks,
Ken