This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVDA100 data rate (bps)

Dear Sir,

I am going to use LIN bus for automotive interface communication and the data rate would be 115200bps  (115kbps).

the specification mention it up to 50kbps. but can it be used for 115kbps? if not do you have any suggestion?  Thanks.

  • Hi passerby,

    The HVDA100 output driver would not be able to achieve 115 kbps signaling, since the output is designed to be slew-rate-limited in order to reduce EMI. The receiver circuitry is able to work at rates >100 kbps, though. Would you need bidirectional LIN communication at this rate, or would receive-only operation of the part be suitable?

    Thank you,
    Max