Other Parts Discussed in Thread: DS34RT5110
Looking for an HDMI interface that can support 1440p resolution. The description for the DS34RT5110 calls out the latest HDMI 1.3 and states: " The latest version, HDMI v1.3, supports a single-link bandwidth up to 340 MHz (aggregate data rate:10.2 Gbps) to support the demands of future HD display devices, such as higher resolutions (1440p), . . ."
However, the DS34RT5110 is NRND. If it is for the latest HDMI, wondering why it is NRND? I don't see any other HDMI devices that show 1440p support - have I overlooked something?
~Leonard