Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TPS2574's GNDG pin issue

Dear All ,

I have to measure the voltage all the pin at the TPS25740 . but GNDG's voltage is fail.   What situation will cause the error function ?

The following is my measurement of voltage, please check.

VTX = 1.1V

CC1 = 0.4V

CC2 = 0.4V

HIPWR = 1.86V

DVDD = 1.86V

VAUX = 3.84V

EN_IN = 2.5V

ISNS = 15mV

VPWR = 5.2V

GDNG = 15mV

GDNS = 15mV

VBUS = 15mV

DC Jack to Type C_20160406.pdf