Other Parts Discussed in Thread: TPS65982
How the heck does one go about programming the I2C address on this device? TPS65982 reference manual section 8.5.2.3 says "The boot code sets the hardware configurable unique I2C address of the TPS65982 before the port is enabled to respond to I2C transactions. The unique I2C address is determined by a combination of the digital level on the DEBUG_CTL1/DEBUG_CTL2 pins (two bits) and the analog level set by the analog I2C_ADDR strap pin (three bits) as shown in Table 9.
But that manual does not explain what the "strap pin" is nor does it explain what the I2C_ADDR_DECODE means. The datasheet is equally as useless. We are planning on using I2C port1. Furthermore, if the "strap pin" is to be used which bit in the I2C address is it?