Other Parts Discussed in Thread: ALP
Test setup: DS90ub947 --- twisted pair --- DS90ub940 --- Android CSI2 input.
I have the above setup. I can (via ALP software) enable the test pattern generators (1360x768) on both the 940 and 947 evaluation boards and see data on a 1366x768 display through the CSI-2 input. I then input an OLDI 1366 x 768 video from a display and feed it into the 947. The data does not show up.
Question: Can TI provide or tell me what is used to verify the 947 OLDI inputs are working properly?
Using ALP, the "linked to video source" is yes, but data is not displayed.
Any help is appreciated.