This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Access three CPU Uart through one RS232



Hi,

Could you recommend solution for below system? Thanks

  • Di,

    What logic or method decides which CPU is allowed to send data?
    Is it OK if all three CPU receive the incoming RS232 data at the same time ?

    Can 4 signal RS232 be used? TX, RX, RTS, CTS (I/O data with simple hardware flow control)
    Is the application DTE or DCE? Is 1990 terms, Computer or Modem?

    I assume the software run on the remote system knows that there are three different CPU out there.