Other Parts Discussed in Thread: TCA9406, TXS0102
Hi,
As per datasheet of TCA9406, Vil specification is mentioned as below
Q1) Please help us in interpreting the VIL value mentioned in the datasheet, is it absolute value of 0.15V OR VCC X 0.15 V?
As per datasheet, any input voltage on TCA greater than 0.15V for logic 0 may cause the TCA to interpret it incorrectly (logic ‘0’ might be considered as logic ‘1’ as the input voltage falls in undetermined state)
We feel that 0.15V for “ VIL max” is very less value as digital circuits are prone to have higher noise.
As per datasheet,TCA9406 is compatible to I2C & SMBus protocol. Below are the I2C & SMBus specifications for ViL as per Page 75 of SMBus Specification, Version 3.0
Kindly let us know the value of “Vil max” to be considered in our design.
Q2) “VIL Max” will be dependent on respective voltage rails or VIL value for both ports depend on VCCA ?
Q3) In our design we have connected VCCA to 3.3V rail & VCCB to 5V rail. In this case what will be the “Vil max” for port A ?
Q4) Which logic family does TCA series belong to ?
Regards
Stephen