Other Parts Discussed in Thread: DS90LV001
Hi
Now, we refer DS90LV001 and we want to confirm the meaning of tSKD1, tSKD3 and tSKD4 with AC test circuits and timing diagrams.
According to the datasheet, AC Test Circuits and Timing Diagrams is described as Figure4 and Figure5.
The AC Test Circuits can be referred as it is.
However, we could not determine tSKD1, tSKD2 and tSKD4 in the timing diagrams.
So, our image is like following pictures.
tSKD1 means to make a bit period longer or shorter in same channel, doesn't it?
Next, tSKD3 and tSKD4 are part to part skews.
Following pictures are our image.
We think tSKD3 and tSKD4 are the similar parameters as the tSKD1 but they have different conditions. Are they correct?
Best regards