Other Parts Discussed in Thread: AM4379, TLK105
Hi,
We are using TLK105LRHBR for 100Mbps Ethernet in MII Mode. In that, We are using pin 29 of PHY (COL(MLED)/PHYAD0) for Blinking LED purpose. And we are using Generic Driver.
Processor used in design in AM4379.
From datasheet of TLK105, it is mentioned that,
"The MLED is not activated by
default, but by register access it can be routed through either pin 17 (allowing more configuration options
for pin 17), or pin 29 supporting two simultaneous LEDs (LED_LINK on pin 17 & MLED on pin 29)." and
"REG 0x0025 (MLEDCR Register) controls the MLED routing and configurations"
But we are not able to change 0x0025 register. By default PIN 29 is going LOW State. So, LED is glowing always. Is there any patch available?