Other Parts Discussed in Thread: TPS2552
We use the attached USB power circuit with TPS2552DRV. An external 5.5V connected to the USB power rail while powered up and enabled creates a reverse current flow that is NOT blocked by the device and no FAULT being indicated. After a disable/enable sequence current remains zero and FAULT becomes active.
This behaviour appears to be in contradiction to the datasheet of TPS2552.
Any idea of what is wrong?
While shorted at the output and current being limited by the device as desired there is also no FAULT indication appearing.
Appreciate any feedback,
Bernd