Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IFMT bits of DS90UB940 des?

I'm wondering how to configure my deserializer to *hopefully* do what I need in regards to image formats.  This might involve the CSICFG1 reg's IFMT bits (input format?).

I have a 1080p SONY FCB-MA130 camera board that outputs PARALLEL 16-bit YCbCr422 (8bits for Y, 8bits for C) at 81MHz.  The serializer solution I found that *might* work is the ds90ub925, which is usually used for RGB888 or lesser, but is LVCMOS compatible at 3.3V.  Then for deserializer I picked the newer ds90ub940 which will convert to MIPI/CSI-2 4-lane, which I need.

The DES expects RGB888 as input on FPDLink usually, but I see these "IFMT" bits on pg65 of the datasheet that might indicate a configurable input format.  I'm looking at setting to "01" for YUV422.  Will this do what I expect?

The MA130 can also output CSI-2, but I don't see a SER from TI that can take this in, and I need this to go the max 15 meters of distance.