Other Parts Discussed in Thread: LMH1983
- What does Wrong_Format mean in user defined format ?
- What frequency range and clock format is acceptable for HIn of LMH1983 user defined format ? Is the rage only within 6-67 kHz ?
regards,
Nobu Furihata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMH1983
regards,
Nobu Furihata
Greetings Furihata-San,
1). LMH1983 counts clock pulses between HSYNC pulses and uses F and V sync to determine incoming video frame format. Valid video frames are listed in table 2 of the data sheet.
2). As you noted the range is within 67 KHz.
I would appreciate it if you could please let me know about this application and provide us with more details.
Regards,,nasser
Hi Furihata,
I think it is possible.
You are going to apply 742.5KHz to HSYNC input. There is PLL1 R Divider register(0x29-0x2A) which divides down Hsync. You can set this register to 0x0B or 11 decimal. Then there is another register PLL1 N Divider(0x2B-0x2C) which divides down the PLL1 27MHz clock. Divided down version of 742.5KHz and 27MHz clocks should be the same to allow PLL1 to lock. PLL1 N Divider(0x2B-0x2C) should be set to 400 decimal or 0x192 hex to get these two clocks to be the same.
Given this, PLL1 should be genlocked to 742.5KHz incoming clock. After this change, you may need to fine tune loop bandwidth to make sure the loop is stable.
Regards,,nasser
Hi Nasser,
Here is my LMH1983 register dump.
Reg 0 = 0x2C
Reg 1 = 0x60
Reg 2 = 0xE0
Reg 3 = 0xC0
Reg 4 = 0x00
Reg 5 = 0x2B
Reg 6 = 0x08
Reg 7 = 0x0E
Reg 8 = 0x0D
Reg 9 = 0x00
Reg A = 0x0F
Reg B = 0x00
Reg C = 0x00
Reg D = 0x00
Reg E = 0x00
Reg F = 0x00
Reg 10 = 0x00
Reg 11 = 0x34
Reg 12 = 0x30
Reg 13 = 0x30
Reg 14 = 0x30
Reg 15 = 0x02
Reg 16 = 0x03
Reg 17 = 0xFF
Reg 18 = 0x01
Reg 19 = 0xFF
Reg 1A = 0x00
Reg 1B = 0x01
Reg 1C = 0x10
Reg 1D = 0x00
Reg 1E = 0x00
Reg 1F = 0x00
Reg 20 = 0x1F
Reg 21 = 0x08
Reg 22 = 0x05
Reg 23 = 0x06
Reg 24 = 0x00
Reg 25 = 0x01
Reg 26 = 0x00
Reg 27 = 0x1F
Reg 28 = 0x05
Reg 29 = 0x00
Reg 2A = 0x0B
Reg 2B = 0x01
Reg 2C = 0x92
Reg 2D = 0x08
Reg 2E = 0x00
Reg 2F = 0x02
Reg 30 = 0x0C
Reg 31 = 0x00
Reg 32 = 0x03
Reg 33 = 0x05
Reg 34 = 0x20
Reg 35 = 0x08
Reg 36 = 0x4B
Reg 37 = 0x02
Reg 38 = 0x00
Reg 39 = 0x16
Reg 3A = 0x49
Reg 3B = 0x00
Reg 3C = 0x01
Reg 3D = 0x0A
Reg 3E = 0x50
Reg 3F = 0x04
Reg 40 = 0x65
Reg 41 = 0x00
Reg 42 = 0x01
Reg 43 = 0x08
Reg 44 = 0x98
Reg 45 = 0x04
Reg 46 = 0x65
Reg 47 = 0x00
Reg 48 = 0x01
Reg 49 = 0x00
Reg 4A = 0x0B
Reg 4B = 0x00
Reg 4C = 0x00
Reg 4D = 0x00
Reg 4E = 0x00
Reg 4F = 0x00
Reg 50 = 0x00
Reg 51 = 0x02
Reg 52 = 0xDE
Reg 53 = 0x02
Reg 54 = 0xD0
Reg 55 = 0x00
Reg 56 = 0x0B
Reg 57 = 0x01
Reg 58 = 0x92
Reg 59 = 0x05
Reg 5A = 0x00
Reg 5B = 0x01
Reg 5C = 0x00
Reg 5D = 0x88
Regards,
Nobu Furihata
Hi Furihata,
I generated 742.5KHz clock and used with LMH1983EVM. I was able to get PLL1 to lock to this clock. Please attached note LMH1983 register settings to enable genlock to this clock in custom mode. In these settings, we are enabling custom mode and over-write registers 0x51 through 0x5D. I Also, EN_AFD needs to be disabled. Also, i multiplied R1 and N1 dividers by 4. Please try these and let me know.
I would appreciate if you could please tell me about the company you work for and a bit more about this application. If you prefer, please send me email at nasser.mohammadi@https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/138/742p5KHz-Custom-Mode-Setting-1.nrdti.com
Regards,,nasser