Other Parts Discussed in Thread: DS10BR150
Hi,
for a new project i want to use your DS10BR150 LVDS Buffer/Repeater.
I have a question regarding termination of this product.
In the data sheet on page 1 i can found the sentence:
"The differential inputs and outputs are internally terminated with
a 100Ω resistor to lower device input and output return losses, reduce
component count and further minimize board space."
In block diagramm on page 2 i can found the symbols for this resistors on
input and output too.
If i have a look on the user manual of the DS10BR150 evaluation kit,
i can found in the schematics (page 6) an extra 100Ohm termination
resistor (R1) on the input of the DS10BR150.
So my questions are:
1. Is this a double termination or does the circuit DS10BR150 not have
an internal 100Ohm terminator? How can i unstand it?
2. If the DS10BR150 have a internal termination resistor on the input,
is this internal termination resistor (100Ohm) biased, so that i can use ac-coupling
on the input of the DS10BR150?
Kind Regard
Torsten