Other Parts Discussed in Thread: DP83867CR, DP83867IR
Hi all
Would you mind if we ask DP83867IR or DP83867CR?
<Question1>
When 25MHz clock inserts to XI with RGMII mode, how much of CLK_OUT output? 25MHz or 125MHz?
Is CLK_OUT possible to output 125MHz always??
In case of 1000Base, GTX_CLK needs 125MHz input.
What is the best way to make 125MHz clock input for GTX_CLK?(is it usual to make 125MHz using PLL of FPGA, isn't it?)
<Question2>
The datasheet shows as followings about power sequence;
When operating in 3 supply mode, the 2.5-V VDDA2P5 can come up with or after the 1.8-V VDDA1P8 but not before it.
It is highly recommended that the 1.8-V VDDA1P8 supplies be powered first.
There is no sequencing requirement for other supplies when operating in 3 supply mode.
Is it possible to power on in the order of 1.8V -> 1.0V-> 2.5V?
Should we power on 1.8V or 2.5 -> 1.0V?
<Question3>
When XI connects to 25MHz crystal, the input XI voltage level is the same as VDDIO, right?
If our recognition uncorrect, please let us know?
Kind regards,
Hirotaka Matsumoto