Hi,
Could you tell me which function following Power supply is used for ?
*VDDA1P0 :
*VDDA2P5 :
*VDDA1P8 :
*VDDIO : (Is it used any function except I/O ?)
Best Regards,
Machida
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you tell me which function following Power supply is used for ?
*VDDA1P0 :
*VDDA2P5 :
*VDDA1P8 :
*VDDIO : (Is it used any function except I/O ?)
Best Regards,
Machida
Hello Machida,
VDDA1P0: 1.0V/1.1V. Core voltage for the PHY.
VDDA2P5: 2.5V. Core voltage for the PHY
VDDA1P8: Optional 1.8V supply. Used for reduced power consumption.
VDDIO: Configurable I/O voltage. Can support 1.8V, 2.5V and 3.3V.
Except for the VDDA1P8, all other supplies are a requirement for the PHY.
-Regards,
Aniruddha
Hi Aniruddha-san,
Thank you for your reply.
You mentioned that "VDDA1p8" is optional 1.8V supply.
Could you please tell me which use case user should use this voltage domain ?
In my understanding, user can use this device just suppling only VDDA2p5.
However, if user can supply both VDDA1p8 and VDDA2p5, user can observe decreasing of power consumption of PHY than single voltage case (VDDA2p5).
Is my understanding correct ?
Best Regards,
Machida