Other Parts Discussed in Thread: DP83848C
In my circuit, I have connected DP83848C to ARM Cortex-M3 LPC1769 of NXP in RMII mode. The Hardware is working fine at 100 Mbps network. There is no pinging problem at all. But when I connect the same H/W at 1000 Mbps network, pinging fails. On an average, out of 10 times, 8-times it is showing 'Request Timeout' . Pls. help to solve the problem .