This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about SN75161B

 

Dear Technical Support Team,

 

I have a question about SN75161BDW.

 

Can input pin(NRFD-16pin, NDAC-17pin, SRQ-12pin)accept High-z?

I worry about that internal transistors are damaged by High-Z.

Datasheet Page.2 describes bellow.

 

------------------------

Each receiver features pnp transistor inputs for high input impedance and hysteresis of 400 mV

for increased noise immunity.

 

Best Regards,

y.i

  • Y.I.

    I do not expect any damage for HI-Z on these pins.
    Do you have any expectation for the pins operate as if they ware low or high when they HI-Z?
  • Hi Ronald Michallick,

    Thank you for your reply.

    >I do not expect any damage for HI-Z on these pins.
    →I understand that.

    >Do you have any expectation for the pins operate as if they ware low or high when they HI-Z?
    →Does it mean that the internal circuit provide low or high level if HI-Z on these pins?
    It's ok that device doesn't any damage for HI-Z on these pins.


    Best Regards,
    y.i