Other Parts Discussed in Thread: TPD4S009, TPD4E001
What is the allowed safe safe of continuous current through an ESD diode?
Alex
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Can a 40 ms exposure to a continuous current flow be a long enough to damage the part
a. This would be dependent on the amount of current, it would need to be very small
2. Can be the same assumption applied to the ESD protection of the SN74LVC2G07DCKR. I guess outputs are ESD protected. There is possibility, in our implementation, for a feedback power flowing through the ESD diodes.
a. Can I see a schematic and a description of the source of the feedback?
Thanks,
Hi Alex,
Okay, I see the issue. The solution is to use the TPD4S009. It is designed to prevent this. There is a blocking diode arranged so that no current will flow with up to 5.5V applied to any data protection pin (these are called IOx on TPD4E001 and Dx in TPD4S009) before any voltage on VCC appears. This is unique to TPD4S009 in our product line. Below I have circled the blocking diode that will prevent the current flowing.
Anything else?