This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DeMux companion chip to DS90UB960 camera Hub Deserializer

Dear e2e,

I would like to use a ds90ub960 camera Hub Deserializer;  4 cameras are connected and the replicate mode shall be used; therefore all four cameras are output in time multiplex on both MIPI CSI2 outputs.

From one of these two outputs I would need to generate 4 single video data streams which can be output via 4 single coax cables. Is there any chip available which can do the time demultiplex and split the output from the ds90ub960 into four separate video channels?


Kind regards,

Uli