This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power consumption of XIO2001

Guru 19685 points

Other Parts Discussed in Thread: XIO2001

Is there information of XIO2001 power consumption (or supply current) on below condition?

・Host: PCI Express ×1 Gen-1

・Secondary: PCI 32bit / 33MHz ×1port

・Bus speed:1Mbps~

【Background】

・When I see the datasheet page 16~17, thermal range is not match on customer condition (Ta:45℃).

・If condition of 1 port, 33MHz, etc, I want to check supply current will decrese more than datasheet P16~17 ,or not decrese. 

Best regards,

Satoshi

  • Hello Satoshi,
    Not with that exactly environment, this is actually why we only provide reference numbers, because every implementation will have specific parameters that will give different power consumption numbers.
    Customer can take the numbers in the datasheet as a reference, if they want to know how much does it really draw in their implementation they will need to measure it.
    Regards